Hello ,
I am having 4 strain gauges in a wheatstone's bridge configuration installed in 45 degrees configuration shown on the photo below on torsion rod.
I am using an instrumentation amplifier with high gain in order to amplify the signal. The voltage signal actually changes correctly with the applied torsion. However , after implementing the same setup on multiple torsion rods , I am getting a reversed voltage change although I am applying the force in the same direction and using the same weight and all the strain gauges are installed in the same directions. By reversed voltage change , I mean that the voltage is increasing on one setup while increasing force on a specific direction and the voltage is decreasing on the second setup while increasing the force in the same direction.
Here are photos for the 2 setups that are behaving oppositely.
I can't find any differences between the 2 setups. I need help from someone who is expert in strain gauges. Note that when I apply force on the other direction of the axe of setup number 1 , it increases. but on the same side like setup number 2 it behaves oppositely.
Thank you very much in advance.
BR
Amr Wael