This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001: ratio

Part Number: OPT3001


We are using your photosensitive sensor, model OPT3001. In actual use, we found that the measured value has a large deviation from the measured value of the standard illuminometer (UT383). We would like to ask if your company has a solution.

My sensor is initialized to a continuous sampling mode with a sampling period of 800ms. The maximum measured value is limited to 5241.60lux (that is, the value of the configuration register register 0x01 is set to 0x7C10).

The measurement method is as follows:

(1) Experimental equipment: light sensor equipment (equipment developed by our company using OPT3001), light meter (UT383, standard light measuring instrument), light source equipment (light equipment developed by our company)

(2) Establishment of experimental environment: the light sensor equipment and the light meter are placed in the same environment, the light source equipment directly shines on the two equipment, adjusts the brightness of the light source equipment, and records the values of the sensor and the light meter.

(3) The measured data are as follows:

Test environment: daily office environment of Tong'an Verification Section Office, SI08B: v1.0.28

Light source: IEM-25BC-TW color temperature 3000K

Illuminometer: Ulead UT383 mini illuminometer

Test method: after the sensor is reset, it is added to the test site. Status configuration: not configured. The default value of brightness sensitivity and deviation is 5%.

The inductor, light meter and light source are placed on the same horizontal plane with a straight-line distance of 23cm.
Light source:
IEM-25BC-TW
Brightness (%)
Illuminometer display data (lux) Sensor Display Data (38B8)
Data before calibration (lux)
Sensor Display Data (38B8)

Data after calibration (5% data calibration, lux)
disparity ratio
0 175 72 170 -5 -2.86%
5 936 299 912 -24 -2.56%
10 1254 391 1349 95 7.58%
15 1558 492 1537 -21 -1.35%
20 1863 579 1854 -9 -0.48%
25 2127 675 2154 27 1.27%
30 2401 760 2438 37 1.54%
35 2669 852 2734 65 2.44%
40 2906 916 3047 141 4.85%
45 3187 1029 3367 180 5.65%
50 3445 1099 3647 202 5.86%
55 3685 1203 3931 246 6.68%
60 3979 1290 4191 212 5.33%
65 4186 1376 4483 297 7.10%
70 4440 1452 4755 315 7.09%
75 4680 1537 5000 320 6.84%