Other Parts Discussed in Thread: FDC2114, FDC2212, FDC2214, FDC2112, TIDA-00317
Hi team,
In our application, we use the FDC1004 sensor to measure the liquid level of the bottle. Use rinse solution - 2ml of rinse additive (surfectant ) and add to the 1ltr of deionized water, Pour 100 ml of the mixed rinse solution into the empty bottle and leave for some time. Shake the bottle at a 50-degree angle and measure the volume of rinse solution. It was observed that it took more than 15 minutes to settle down the capacitance value. When I use tap water or deionized water to measure the capacitance value from the sensor, it takes 40 seconds to settle down the capacitance value.
I believe this is a FDC1004 sensor IC issue, can you suggest a way to reduce the settling time or how to use the sensor to detect soapy water with foam?
Thanks,
Sathya. D