Other Parts Discussed in Thread: LDC1101
The LDC1101EVM eval board allows the user to configure the voltage supply for the LDC1101, either 1.8V (default) or 2.5V. The datasheet specs the LDC1101 at Vdd=1.8V, and states that the device can be powered between 1.71V to 3.46V. The datasheet doesn't explain how performance is affected at supply voltages other than 1.8V. The graphs in the datasheet show that higher voltages result in increased current draw which is no surprise, but they reveal nothing about measurement performance.
My question is, will higher voltage supplies (within the acceptable supply range) have significant performance effects on the LDC1101?