Other Parts Discussed in Thread: OPT3007, TAS2505
Hi Team,
Could you please help share the kernel and user mode driver in source code? Thanks.
Regards,
Hailiang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hailang,
You can find information on the drivers for our entire family of light sensors at the link below.
Rahland Gordon
Hi Rahland,
Thanks for you information, I have a few questions:
• Is there any example of DTS node for your driver?
• I didn’t see any node parse code in the driver.
• And I also see there is interrupt handler in driver, where to set the interrupt GPIO?
Regards,
HL
Hi Hailiang,
Can you elaborate what you mean by "node"? The C++ driver can be configured to work with 3001,4,6, and 7 by updating the TI_OPT3007_BUSADDRESS defined on line 15 of opt3007_hostControl.h.
Which driver are you referring to with the interrupt handler?
Thank you,
Brent Elliott
Hi Brent,
The node the customer mentioned is the device tree node in dts file of Linux driver.
For example: tas2505 is a node of sound card driver
Is there such sample for the light sensor?
Regards,
Hailiang
Hi Hailiang,
I am unaware of an equivalent for OPT, but just an FYI, our Linux driver will have limited support as the driver that we can support and recommend will be the C++ driver.
Thank you,
Brent Elliott