Other Parts Discussed in Thread: IWR6243
Hi,ade
I am trying to perform profile configuration for the IWR6243 RADAR (57GHZ to 64GHZ), RADAR sends error code 46 [Ramp end frequency is not within [76, 81] GHz], the profile configuration values I took directly from the DFP example codes.
ptrProfileCfg->profileId = 0;
ptrProfileCfg->startFreqConst = (uint32_t) ((float)57.02 * (1U << 26) / 2.7);
ptrProfileCfg->idleTimeConst = 14 * 1000 / 10;
ptrProfileCfg->adcStartTimeConst = 6 * 1000 / 10;
ptrProfileCfg->rampEndTime = 67.04 * 1000 /10;
ptrProfileCfg->txOutPowerBackoffCode = 0;
ptrProfileCfg->txPhaseShifter = 0;
//ptrProfileCfg->freqSlopeConst = 11 * 1000 / 48;
ptrProfileCfg->freqSlopeConst = (16.9824*(1<<26))/(2.7 * 1e3 * 900);
ptrProfileCfg->txStartTime = 1 * 1000 / 10;
ptrProfileCfg->numAdcSamples = TEST_NUM_ADC_SAMPLES;
ptrProfileCfg->digOutSampleRate = 10000;
ptrProfileCfg->hpfCornerFreq1 = 0;
ptrProfileCfg->hpfCornerFreq2 = 0;
ptrProfileCfg->rxGain = 30;
These are the values, Please suggest a solution for fixing this error.
Regards,
Surya
Regards,
Surya