Other Parts Discussed in Thread: UNIFLASH, MMWAVEICBOOST, , IWR6843ISK, IWR6843
Hello everyone,
I recently purchased the IWR6843ISK-ODS mmWave sensor evaluation kit, along with the carrier card platform mmWaveIcboost. I am excited to explore its capabilities and start working on my project. However, I have encountered a problem while trying to load firmware onto the IWR6843ISK using Uniflash.
When attempting to use Uniflash, I encountered the following error message:
"[ERROR] Cortex_R4_0: Serial port /dev/ttyACM0 specified does not exist, is already open, or permission is denied!!"
This error has left me wondering whether the device is broken or if there is a misconfiguration issue. I'm not sure if the error message indicates a problem with the hardware, such as a faulty serial port or a misconfigured connection, or if it is related to software settings. For every try I pressed the NRST button and even tried to disconnect the board entirely from my PC and power supply, but with no results
I have double-checked the physical connections between the IWR6843ISK and the carrier card, ensuring they are properly connected. Additionally, I have verified that the required drivers are installed on my computer. Despite these precautions, I am still unable to successfully load the firmware using Uniflash.
I'm reaching out to the community for any suggestions or insights that could help me diagnose and resolve this issue. Has anyone encountered a similar problem with Uniflash and the IWR6843ISK-ODS? If so, I would greatly appreciate any guidance on troubleshooting steps or potential solutions.
Here are a few specific questions that come to mind:
Could this error be caused by a misconfiguration in Uniflash or any other software settings? If so, what are the possible areas I should check and adjust?
Is there a way to verify if the IWR6843ISK-ODS device itself is functioning correctly? Are there any diagnostic tests or tools I can utilize to ensure its proper operation?
Are there any alternative methods or tools available for flashing firmware onto the IWR6843ISK-ODS that I can explore as a workaround?
I would be grateful for any advice or suggestions from those who have experience with the IWR6843ISK-ODS and Uniflash. Thank you in advance for your assistance!
Best regards,