Hi,
I'm using Long Range People Detection example in Radar Toolbox 1.0.1.7
Works well when using the binary provided as a prebuilt.
I imported and used the example into CCS to modify baudrate, and found that the incorrect target info was output.
(Same even if baudrate is not modified)
Below is a part of the data parsing result that I implemented.
Below is the result when executed with the provided industrial visualizer.
Are there any reported bugs related to this?
Thanks.