Other Parts Discussed in Thread: OPT3001
Hi TI Team,
We are interfacing TI's opt3004 ALS with the Ambarella CV25 Processor. We are using the driver code - "opt3001.c" and it was loaded perfectly.
We have using gpio 44 as the interrupt and configured in the device tree .
Device Tree Configurations -
opt3001@44 {
compatible = "ti,opt3001";
reg = <0x44>;
interrupt-parent = <&gpio>;
interrupts = <44 IRQ_TYPE_EDGE_FALLING>;
};
But the pin is not working as an interrupt.
Also providing the value of lsiio command
# lsiio
Device 001: opt3001
Device 002: e4003000.adc
Device 000: Main
Trigger 000: e4003000.adc-dev2
Kindly check and give a solution to work the gpio as the interrupt.
Thanks,
Abhiram