Other Parts Discussed in Thread: IWR6843AOP, MMWAVEICBOOST, , CC3220S
Hi there,
I am working on a project to design a fall detection system for the elderly that sends a SMS message to a caregiver/family member when a fall is detected. I recently purchased both an IWR6843AOP evaluation module and a MMWAVEICBOOST carrier card, and so far I have flashed the IWR6843AOPEVM with the 3D_people_count_68xx_demo binary to run the 3D_People_Counting lab along with the Fall Detection GUI. I am happy with the sensing capabilities that were demonstrated, so the next step I would like to take is sending the alert SMS message.
At this stage, I would like to try to use Wi-Fi as the communication protocol. My question has two parts:
- As mentioned, I currently have an IWR6843AOPEVM and a MMWAVEICBOOST. What other hardware might I need that would enable the sensor to be Wi-Fi enabled and programmed to send a message when a fall is detected to a caregiver/family member's device on the same Wi-Fi network?
- Is there any software available that works well with TI hardware that can be used to send SMS messages after an event is triggered? Something I came across was using Temboo and calling the Twilio API to send a SMS message after the event trigger, but I am not 100% sure if that would work with the current hardware I have (here is link to the Temboo example: https://temboo.com/hardware/ti/send-sms).
For reference, this video (https://www.youtube.com/watch?v=R_kCVP2ni14) from TI demonstrates something similar to what I have in mind for the mounting setup and the messaging service of my fall detection system project.
I appreciate any guidance/help.
Thank you!