我们首次测试,探测距离3mm,天线直径13.9mm。
因结构限制,探测距离要增加到8mm,根据比例计算,天线直径需要做到37.2mm以上,那么检测精度还能跟之前保持一样吗?
你们有类似的探测距离在8mm左右的应用吗?
除了正后方和侧方不能有金属,其他设计还需要注意些什么?
---
Our first test, the detection distance is 3mm, and the antenna diameter is 13.9mm.
Due to structural limitations, the detection distance has to be increased to 8mm. According to the ratio calculation, the antenna diameter needs to be more than 37.2mm, so can the detection accuracy remain the same as before?
Do you have similar applications where the detection distance is around 8mm?
In addition to no metal on the front and side, what else should be paid attention to in other designs?