Other Parts Discussed in Thread: FDC1004,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Huangjian,
A few questions about the analog part of the design:
1. What are the dimensions of your sensors?
2. What is the physical spacing between your sensors?
3. What are your sensor frequencies?
4. Do the results change for a single channel if all of the other channels are off?
Just so you know, we recommend the FDC1004 over the FDC2xxx devices, especially for liquid-level sensing.
The FDC1004 features active shield drivers, which help with EMI management, while many of our customers have struggled with EMC/EMI issues with FDC2xx devices.
You can find out more about the FDC1004 at the FDC1004 product folder and on the E2E FDC1004 Frequently Asked Questions age.
Regards,
John
Hello John Miller
The length of the sensor extending outward is 100mm, and the impedance is 42KΩ。
The spacing between probes is 9mm。
We use frequencies at two frequency points: 4.6MHz and 5.1MHz。
Single channel detection is stable and has no impact。
May I ask if there are any good suggestions for design besides selecting the
FDC1004 chip?
Huangjian,
What is the liquid used in your reported results?
The single-channel amplitude data looks like it moves between the values of -4500 to -3500, while the multi-channel measurement ranges from 8000 to 14000.
If the two data sets were taken for the same probe and position, it appears the capacitive sensors may be interfering with one-another.
You mentioned sensor frequencies of 4.6MHz and 5.1MHz.
1. Are the two frequencies used in alternating probe positions?
2. The schematic is a little fuzzy, but it seems to show the antenna connected to INxA and the reservoir connected to INxB.
What are the details of the INxB connection?
3. What are the Qs of the resonant antennas + PCB inductors for the two frequencies?
4. What is the inductance and self-resonant frequency of your PCB inductor?
regards,
John
Hi
FDC2212 Engineering Application Technology Consulting
There are many types of liquids, including polar and non-polar molecules
We have tried to verify that channels 2, 4, 6, 8, and 1, 3, 5, and 7 use 4.6MHz and
5.1MHz respectively, resulting in a slight reduction in interference.
frequencies?
Our antenna probe is 40K Ω and the inductance is 18uH, but we are not sure about
the internal circuit of the chip, so we cannot accurately evaluate it
We use an inductor of 18uH and a capacitor of 18pF, resulting in a frequency of
around 5.1M;The inductance is 18uH, the capacitance is 33pF, and the generated frequency
is around 4.6M.
Huangjian,
Two potential causes come to mind: