This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5173-Q1: under-voltage

Part Number: TMAG5173-Q1

Hello,

as i am working on ultra low consumption design, i would like to understand well the of the test description column corresponding to the "Under voltage threshold at VCC" line. That is to say "Internal parameter (OTP option)".

What does that mean ? Is it related to B, C and D versions of TMAG5173 ?

Furthermore, what should be the minimum voltage ? I saw that it is written many time in the datasheet that the TMAG starts up at 2.3V but figures 6-2 and 6-4 show 1.8V sense performing. But what is the minimum ?

Best regards.