Other Parts Discussed in Thread: IWR6843, IWR6843ISK, , MMWAVEICBOOST
Hi, I am trying to use DCA1000EVM Data Capture Card to capture raw data generated by iWR6843ISK board. In my setup, I have the iWR6843ISK board connect to mmWave ICBoost board. When I open the DCA1000EVM user's guide, it only includes guidelines to capture data from iWR1xxx EVM, doesn't mention how to capture data from iWR6843 at all. I have two questions here:
1. Can I use DCA1000 to capture data from iWR6843ISK? If I can, how should I do it? Is there a user's guide for that?
2. In the DCA1000 user's guide, it seems the raw data can only been stored to a file, then I can use other software to open the file and analyze data. Is there way to send the raw data file to software such as Matlab etc. in real time? What I want to implement is to use iWR6843 to detect a moving object, then real time generate a signal in Matlab or some other programs.
Thanks,
Hank