Other Parts Discussed in Thread: TMP236
Hi,
We use the TMP20 in a temperature control application which is set to 30 °C.
The temp error at 30 °C is between 0.8 % and 1 %.

The max deviation (error) around 30 °C is 0.004 °C.

Accuracy vs supply is given as 0.05 °C/V which translates to 0.076 °C at 1.5154 V (30 °C).
What is the accuracy at this temperature? How is it calculated around 30 °C?