Part Number: DRV5032
Customer would like to know that what max. voltage derating Vdss of the open-drain output? Could you help to answer! Thanks.
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV5032
Customer would like to know that what max. voltage derating Vdss of the open-drain output? Could you help to answer! Thanks.
Regards
Brian
Brian,
Thank you for reaching out on E2E. The absolute maximum rating for this device is shown here:

Vcc is rated to 5.5V, and the output voltage is rated to VCC+0.3V. So under no case should the pull-up voltage exceed 5.8V. However, we never recommend using a different voltage for the pull-up than VCC. It is best to connect the pull-up resistor directly to VCC at the device to ensure that the Output voltage rating is never at risk of being violated.
Thanks,
Scott