Other Parts Discussed in Thread: IWR1443
Dear Sir
I would like to confirm or ask the following questions regarding your answers.
1. Answers and questions to your question "Do you have your device in functional mode?"
The dip switch of IWR1443BOOST is set to functional mode [SOP0: short circuit, SOP1: open, SOP2: open]. What else do I have to do besides this?
2. Questions regarding the operation of IWR1443BOOST
The mmwave demo visualizer is working properly, so the firmware has been installed correctly on the IWR1443BOOST.
After that, I send a profile (for example, profie_2d.cfg) that describes "sensorStop to sensorStart" from the PC to IWR1443BOOST using another application (CLI teraterm or my own program created with Python, etc.),
but there is no response. What should I do to return data from IWR1443BOOST?
Please let me know regarding the above 2 items.
3.The settings related to the connection COM port are as follows.
①. <Transmission>XDS110 Class Application/User UART Port: COM5, baud rate: 115200, byte size: 8 bits, stop bit: 1, parity: none, timeout = 1, (xonxoff, rtscts, dsrdtr) not set
②. <Reception> XDS110 Class Auxiliary data Port Port: COM4, Baud rate: 921600, Byte size: 8 bits, Stop bit: 1, Parity: None, Timeout = 1, (xonxoff, rtscts, dsrdtr) are not set.
Thanks with Best Regards.
H.Imabayashi