Hi champs,
Customer have questions regarding to fallback scheme if RBL detect Image is corrupted.
1. What kind of scheme to check wither image is corrupted or not? CRC for each image embedded in each .RPRC? or just overall CRC appended at the end of multicore image .APPIMAGE?
2. The image format in TRM 4.7 Boot Image Format is inconsistent with TOOLS_BOOT.html of the SDK. In TRM every image in RPRC file has its own CRC. Will RBL check every CRC (including the Meta Header, core Images) in the header is correct? If yes, it means any bit flip on the meta header or on the image in RSRC format in the flash will load failure? Or just put CRC there, just do nothing?
3.What does RBL do when the loading failure? reloading on next METE partition or just load next appimage from META IMAGE2, META IMAGE3 ...? Any log information?
4. The table of register in the TRM 4.6.2.5.7 show the status which having load failure, Can HOST query these statuses via the UART used to update firmware?
Regards
Andre