Hi
If we just need the raw data capture, what the signals can be omitted in the following connector I/F ?
Thanks
Michael Su
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
If we just need the raw data capture, what the signals can be omitted in the following connector I/F ?
Thanks
Michael Su
Hi, Michael:
Please give us a day to get back to you.
Best,
Zigang
Hi Micheal,
For raw data capture other than I2C signal all the other signals are necessarily needed. We would recommend to have I2C also as it will be an interface to PMIC.
Thanks,
Kundan
Hi,
Could you tell us the following signals are for what between the DCA1000 and AWR6843 ?
could you explain their function in more detail ?
SPI, I2C, RS232, AR_RESET_POR_N, AR_SYNC_IN, PGOOD,
Thanks
Michael Su
Hi Micheal,
SPI is used to send commands from studio to MSS application which calls mmWavelink APIs.
RS232 is used to download the firmware when using the mmWave studio.
I2C will be used for setting the PMIC configurations.
Pgood is an LED indication.
AR_RESET is to give the reset assertion from mmWave studio.
Thanks,
Kundan