Other Parts Discussed in Thread: TMAG5170
Tool/software:
Hello! I'm seraching for a magnetic sensor with high analog bandwidth for measuring flux of ~15 ... 100mT(or less) @ up to ~8kHz and with SPI or I2C. I want to measure up to the 36xharmonics of a 50Hz system and create a spectrum visualization. It has to have a temperature rage of minimum -40°C ... +85°C and work at 3V3, 3V6 or 5V and is available on the market. Is this possible with TMAG5173-Q1 or should i use another sensor? Thank you!