This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: BSS CPU Fault Async event

Part Number: AWR2243

Tool/software:

CPU information as follows:
gCLIMMWaveOpenCfg.frontEndCfg.csi2Cfg.lanePosPolSel = 0x35421
MmwDemo_openSensor start
Debug: CLI is operational
EDMAself_test[1] slavePowerUp success
MmwDemo_openSensor success
B1 SLAVE_PHASE_CHANGE
[C66xx_DSP] DPC_OBJDET_IOCTL__STATIC_PRE_START_CFG
[Cortex_R5_0] MmwDemo_configSensor success
failed:Dv_Mon_init
MasterDevIdx:0
u8DevMap:2
ptrMMWaveMCB->deviceMap:3
Device map 0 : BSS CPU Fault Async event
3, 2045, 17724, 0, 287, 134282960, 0, 65535, 255, 255, 255, 255Exception: mss/APP/swc_rf/swc_rf.c, line 105. ASSERT: 31.220092s: mss/APP/swc_rf/swc_rf.c:MmwDemo_eventCallbackFxn:105: 0 failed !!!