Tool/software:
Dear TI Engineer,
Our FPCA product uses OPT3001DNPRQ1 as the light sensor for vehicle, but the device ID read by different end customers on the same device is different. The Tier1 manufacturer read the device ID is 3001h, which is consistent with the Device ID on the datasheet, but the Device ID read by the automobile factory is 3000h with the same product.
The I2C waveform captured by our logic analyzer and oscilloscope can also indicate that the device IDs read are different.
The waveform captured by Tire1 is as below:
The waveform captured by automobile factory is as below:
Can you help analyze the cause of the problem?
Thanks,
Kind Regards