Other Parts Discussed in Thread: TDC1000
Tool/software:
Hello!
I am looking for a method to have more flexibility over the clock speed of the TDC1000 chip. Is there any way that the evaluation board can be manipulated so that we can sweep through frequencies instead of only having one 8 MHz clock speed? I am familiar with the ability to divide the clock speed by different divisors in the GUI, but I was hoping to have a much more refined adjustment of the frequencies to be able to better match the output frequency from the evaluation board with the ultrasonic transducer and also to optimize the frequency so that the ultrasonic waves can better penetrate through 304 Stainless Steel, the material of the container I need to use. Does the board have the capabilities to implement a phase lock loop?
Thank you!