Other Parts Discussed in Thread: IWRL6432
Tool/software:
Hi Ti Team,
Unfortunately, I am having problems getting started with MMWAVE Studio + DCA1000 Capture Card + 6432AOPEVM.
I followed the instructions in the current SDK and was unfortunately only able to establish a partial connection.
The feedback from MMWAVE Studio does not correspond 100% with the images in the SDK instructions. I select following files:
C:\ti\MMWAVE_L_SDK_05_04_00_01\firmware\mmwave_dfp\rfevalfirmware\appss\mmwave_plt_rfeval_rprc.bin
C:\ti\MMWAVE_L_SDK_05_04_00_01\firmware\mmwave_dfp\rfsfirmware\xWRL6432\mmwave_rfs_patch_rprc.bin
The first file is transferred successfully but the Firmware Version seems not correct?! During the second transfer, the program stops.
The Device 6432 is not Listed. Which Device am i supposed to select? Did i select the correct Firmware files?
I tried my luck with the newer MMWAVE version. This is the result:
The firmware transfer works. However, the further steps to start the ADC stream fail.


I would be very grateful for any help. Best regards Tobias