Tool/software:
Hello E2E Community,
We are currently exploring LMT87 for our temperature measurement use case, where we have to measure the temperature of the bearing which is about 2-3m away from the MCU board.
We are planning to use a high gain TO-92 package sensor - LMT87 from TI's analog sensor portfolio for this use case.
Kindly guide us if we can convert the 3-wire interface of this sensor into a 2-wire configuration by connecting the voltage output at the sensor side to the Vcc via a suitable resistor?
Also can you guide us on the RC filter that we plan to install on the ADC side? Our current plan is to use a RC based LPF with R: 10kOhm & C: 0.1uF.
Kindly guide.