This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT87: Converting 3-wire into 2-wire for 3m long cable transmission over twisted pair

Part Number: LMT87

Tool/software:

Hello E2E Community,

We are currently exploring LMT87 for our temperature measurement use case, where we have to measure the temperature of the bearing which is about 2-3m away from the MCU board.

We are planning to use a high gain TO-92 package sensor - LMT87 from TI's analog sensor portfolio for this use case.

Kindly guide us if we can convert the 3-wire interface of this sensor into a 2-wire configuration by connecting the voltage output at the sensor side to the Vcc via a suitable resistor?

Also can you guide us on the RC filter that we plan to install on the ADC side? Our current plan is to use a RC based LPF with R: 10kOhm & C: 0.1uF.

Reference Design for 3-Wire to 2-Wire configuration

Kindly guide.