Other Parts Discussed in Thread: DCA1000EVM, AWR6843AOPEVM
Tool/software:
Hi,
I've been evaluating the AWR6843AOPEVM together with a DCA1000EVM using mmWave Studio. For this, I put a radar reflector at several known distances (1-3m). As config, I use the default values.
However, the range amplitude plot did not show peaks where I expected them at all. After some trial and error, it occurred to me that the range resolution calculated in the post-processing divided by 10 would give more reasonable, but still not sufficient, results. See images below where the reflector is moving between appr. 1.17m and 3.06m. The first diagram uses the range resolution calculated by mmWave Studio (19,53cm), for the second this value was divided by 10 (so 1,95cm).

Is there an explanation for this?
Thanks in advance!