This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: CAN data output error

Part Number: AWR2944EVM


Tool/software:

Hi team,

we're using AWR2944EVM with OOB object data over CAN sample project from radar toolbox where we found strange behaviour in the code. for which I need to ask some question.

Question-1:

Why error line from pre-built binary of CAN demo don't match with CCS built and run. because UART process not completed error occurred but in two different line for example given below pre-built binary had this error in line 2800 and ccs at 2798, I just wonder during the update process line has been cut off or something else.



Question-2:

I have tried the OOB data over can project using different version of ccs for example 1220,1240,1260,1270,1271 with SDK version of 4.4.1.2 and radar toolbox version 2.20.0.5, 2.10.0.4, 2.0.0.6, 1.30.1.3 where the error remains the same, I have doubted the installation process what I have done and reset the PC and installed as per the instructions given in api_guide_awr294x, the tried the same process but error remains the same, for hardware connection, I used two different connection for checking.

Hardware used - PCAN-FD from peak systems
connection - 1:
CANA_H - CANH
CANA_L - CANL
GND - GND

during this connection state only, I am getting the error mentioned above. and one data packet 0C1h is received.



connection - 2:
CANA_H - CANL
CANA_L - CANH
GND - GND

during this connection state, I don't see any of the data coming from CAN using peak view.

I have double checked for connectivity and lose contact but there is no such thing.

Also for switch cfg S1 - XDS mode, S2 - PMIC SPI mode

also I have tried to run the demo in ccs but error follows


I am sending the cli without enabling heatmap only.
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 15 0
adcCfg 2 0
adcbufCfg -1 1 0 0 1
lowPower 0 0
profileCfg 0 77 7 7 20.81 0 0 8.883 0 384 30000 0 0 36
chirpCfg 0 5 0 0 0 0 0 15
frameCfg 0 5 128 0 384 50 1 0
guiMonitor -1 0 0 0 0 0 0
cfarCfg -1 1 3 16 0 0 1 24.0 0 7 0 1
cfarCfg -1 0 3 16 0 0 1 15.0 0 7 0 0
compressionCfg -1 1 0 0.5 8
intfMitigCfg -1 15 18
localMaxCfg -1 6 40
antennaCalibParams 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1
measureRangeBiasAndRxChanPhase 0 1.5 0.2
analogMonitor 0 0
calibData 0 0 0
aoaFovCfg -1 -90 90 -90 90
sensorStart

For quick debug we have tried to increase the frame periodicity but not helped it. 

Also during checking for other e2e post someone faced same error but I didn't see how the error has been solved.
e2e link : https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1369944/awr2944evm-sample-applications-not-working
e2e link : AWR2944EVM: CAN output - Sensors forum - Sensors - TI E2E support forums
e2e link : AWR2944EVM: Cannot configure non-standard baud rate 3125000 in Linux Environment - Sensors forum - Sensors - TI E2E support forums

The above mentioned e2e links are the threads whose faced similar error, could you please instruct us where or what we're doing wrong.

Regards,
Deepan