Hi,
I am about to design an AFE4405 based PR/SiO2 board, after seeing the datasheet, the following issues need to be clarified.
Could anybody advise?
1) Can I use a single 3.3V power supply for both TX_SUP and RX_SUP ?
2) To handle interrupt events, can I use either ADC_RDY or PROG_OUT1 ?
3) Regarding clock, should I use an external clock ? According to the AFE4405EVM, the clock was from MSP430. The afe4405 has an internal clock.
Regards,
Konan Kim