This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4400: AFE4400 CALIBRATION FLOW CHART

Part Number: AFE4400

Hi,

I am going through the AFE44XX GAIN CALIBRATION ROUTINE flow chart. I have few questions as below:

1. The TARGET_THR = 33%. Is it 33% of the ADC full scale voltage(1.2 V)? In that case it would be 0.396 V. In the data sheet, it is recommended to be around 80% of its full scale value. Which one is the correct one? Please, clarify.

2. Also, it is suggested to have two parallel routines for LED1 and LED2. For LED1, the concerned register(TIAGAIN, Address =  20h) and for LED2, the concerned register(TIA_AMB_GAIN, Address =21h). But for AFE4400, TIAGAIN register(Address=20h) is reserved for factory use. In that case, how I can calibrate LED1? In that case, is register 21h is responsible for calibrating both LED1 and LED2? And how it works then?

Regards.

Nazrul

  • Hi Nazrul,

    AFE4400 datasheet says that we should limit our signal level below 1V (i.e. 80% of 1.2V). But the calibration routine sets the target as 33% which is below 80 % of full scale. So both the statements are correct.
    Since AFE4400 has single TIA_Gain control for all the phases, you have to use the same gain for both the phases. You have to adjust the LED currents such that you get the required DC ( as defined by target level) with common gain.

    Regards,
    Prabin
  • Thanks Prabin. Regards.
    Nazrul