Other Parts Discussed in Thread: FDC2214, LDC1314
Hi !
Is it possible to use multiple FDC22114 on the single I2C of micro controller for 50 Nos of capacitive touch in following configuration,
1. In 1:1 channel and touch key configuration where on one channel is representing one key, like in this case FDC22114 is having four touch channels, therefore we can have maximum four keys in 1:1 proposition
2. In Matrix touch channel configuration, ie let us say 8X8 matrix which will use required only two numbers of FDC2214 on each side row and column, therefore total 4 FDC2214 will be required for 64 keys.
Note: ( as there are only two hardware address per FDC2214 that is 0X2A and 0X2B, and I think we cannot change them dynamically by switching Address pin IO high/low to address in multiplexed format)
Please advice !
Thanks and Best Regards,
VK