This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are designing distance measurement sensor using capacitance principal using FDC1004. The sensor plate size we are using is 15cm x 10cm copper plate. Shield size is as same as sensor(overlapping principle- Shield and sensor plate overlap each other). Problem we are facing is
1) Sensing area is not unidirectional. We are using shield for restricting sensing area on one side but shield side is still sensitive to object in near proximity zone( 5cm ).
2) Short distance- Plate area is 15cm x 10cm, which is quite big, but we are getting maximum range as 15cm.
3) If we add the ground plate of same area as shield and sensing plate then we are getting 10cm range.
Please share your thoughts on how can we get maximum possible range with above configuration.
Thanks Chris for prompt response!!!
We are taking care of the traces from sensor to device using shield. The composition of the material is fixed for testing purpose. Is there any way through which we can increase the Electromagnetic field and achieve maximum distance.
Any specific sensor design pattern that could give maximum EMF and range? I have seen whitepapers from TI, it mentioned 50cm range achieved. Could you please share any document related to their sensor design if possible.