Hello,
Sorry for the late reply as I worked on a different project last month. Now I'm back to this issue...
I have tried sending CLI config while the device is in CCS debug mode and I notice that the problem occurs in the SensorStart part. Please see below log from CCS when I send CLI config from my own C program:
[Cortex_R4_0] **********************************************
Debug: Launching the Millimeter Wave Demo
**********************************************
Debug: MMWDemoMSS Launched the Initialization Task
Debug: System Heap (TCM): Size: 65536, Used = 2832, Free = 62704 bytes
Debug: MMWDemoMSS mmWave Control Initialization was successful
[C674X_0] Debug: Logging UART Instance @00814ad0 has been opened successfully
Debug: DSS Mailbox Handle @0080c568
Debug: MMWDemoDSS create event handle succeeded
Debug: MMWDemoDSS mmWave Control Initialization succeeded
Debug: MMWDemoDSS ADCBUF Instance(0) @00814ab8 has been opened successfully
Debug: MMWDemoDSS Data Path init succeeded
Debug: MMWDemoDSS initTask exit
[Cortex_R4_0] Debug: CLI is operational
Debug: Heap before creating a tracker
Debug: System Heap (TCM): Size: 65536, Used = 27864, Free = 37672 bytes
Debug: (GtrackModuleInstance *)0x8008a00
Debug: System Heap (TCM): Size: 65536, Used = 50344, Free = 15192 bytes
Debug: MMWDemoMSS Received CLI sensorStart Event
Error: MMWDemoMSS mmWave open configuration failed [Error code -203554190]
I tried adding 2 seconds delay between trackingCfg and SensorStart command but to no avail. Please help explain the Error Code highlighted.