TI E2E Community,
I am using LDC1612 to measure the inductance of the coils of a variable reluctance differential pressure transducer.
The inductance of the coils is roughly 18 mH, and the nominal capacitance of the capacitor that I soldered on is 560 pF which results in a sensor frequency of roughly 50 kHz.
This is how it is set up:
The problem I am having is that there are large glitches that occur in the measurement. Such as the following (250 Hz sampling rate):
When I probe the INA or INB pins, I see the following:
It looks like what I think it should look like except that there seems to be an "extra" oscillation that occurs occasionally at the end of the measurement (In the image above, it is the slightly grayed out one).
The deglitch filter is set on the lowest frequency.
My questions are:
1. What could be the cause of the glitches?
2. Is the extra oscillation that occurs at the end of the measurement a concern?
Thank you
Henri Bouchard