Other Parts Discussed in Thread: DCA1000EVM, , UNIFLASH, AWR1243, MMWAVE-STUDIO
I am attempting to connect AWR1243Boost + DCA1000EVM combo to my computer and to run the basic demo lua.
I have completed the driver installation as instructed and when powered on and USBs connected the device manager correctly shows the 6 com ports. See picture.
SOP 0 and SOP1 are closed; SOP2 is open.
I then start mmWave Studio, and select COM11 as the RS232 Comm Port. The FTDI Connectivity Status shows "Connected." Then I click Set(1) and Connect(2).
Every time, the RadarAPI reports Error: Connection failed: Calling_ConnectTarget returned 3
I have tried restarting the computer, the DCA1000+AWR1243boost combo, and reinstalling the XDS emulation software (versions 8.0.903.4 and 8.0.803.0).
I have also tried a whole other set of DCA1000EVM+AWR1243boost. The error occurs for both sets of boards. Both AWR1243s are ES3,0.