Hi champion,
In function 'SOC_setMSSLinkState', I find it operate register SPARE1, but I could not find this register definition in TRM. Could you help to give this information?
Thanks,
Adam
int32_t SOC_setMSSLinkState(SOC_Handle handle, uint8_t state, int32_t* errCode)
{
SOC_DriverMCB* ptrSOCDriverMCB;
int32_t retVal = 0;
/* Get the pointer to the SOC Driver Block: */
ptrSOCDriverMCB = (SOC_DriverMCB*)handle;
if (ptrSOCDriverMCB == NULL)
{
*errCode = SOC_EINVAL;
retVal = MINUS_ONE;
}
else
{
/* Set the operational status for the MSS */
ptrSOCDriverMCB->ptrTopRCMRegs->SPARE1 = CSL_FINSR (ptrSOCDriverMCB->ptrTopRCMRegs->SPARE1,
18U,
18U,
(uint32_t)state);
}
return retVal;
}