This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7201-ZAX-EVM: Send command to MSP via Backchannel UART

Part Number: TDC7201-ZAX-EVM

Dear all

I`ve got the TDC7201-ZAX-EVM and writing currently an enhanced GUI by myself to enable some functionality i need within my project.

Now i`ve got one question. I`ll get the TOF data via UART backchannel (enable uart stream), working fine. But are there any commands that I can send to the MSP, such as "start" and "stop" or one_shot function?

I checked the firmware files uart_commn.h / .c but i can`t find anything that handles data from UART. Just want to be sure that this is correct and i have not missed something.

Thanks & regards