Part Number: TDC1000-GASEVM
The mode 2 of the TDC1000-GASEVM does not work,
The channel that is selected in the drop down list (CH_SEL) continuously transmits and the other receives, there is no channel swapping observed even though the channel swapping (CH_SWP) is enabled using the GUI.
Initially, we thought it is a hardware issue and thus, bought a new board. But the issue still persists. We have also re-installed the TDC1000_7200 EVM GUI v1.2.7.1 (Rev. F) but it does not help.
All the signals were probed and it was observed that the TX pins, that is pin no. 27 and 28 of the TDC 1000 IC shows the existence of the 5V drive signal only at one channel based on the channel selected in the GUI, and the other channel shows 0 V, that is there is no swapping.
I would be highly obliged if you could help me resolve this issue.