Hello!
I am currently trying to receive a fixed pattern from the radar board, but it seems I am not getting the same pattern I configured on mmwaveStudio 1.0.0.0. I have attached the configuration I have used, knowing that my ADC sampling rate is 10MSps. I have left the offset field set to null, assuming that this configuration will just send first the pattern, and I have set the added values to I = FFFF and Q = 0000, respectively (to see the differences between the phases). Now, I expected to obtain on Wireshark some UDP packages containing just FFFF and 0000 all over, but I got nothing like I thought and commented when analyzing the first packages. I guess the configuration is not properly set, but I can not find too much documentation or guidance on configuring test pattern in mmwaveStudio. It would be helpful if you provide documentation on how to set these parameters or, at least, an example on how to configure the mmwaveStudio pattern generator and what we should expect as outcome on the UDP packages.
Thank you,
Gorka