Other Parts Discussed in Thread: AWR1642
I have been using Radar studio to collect raw ADC data from the AWR1642 using the devPack and Tsw1400. The data all looks good using the built-in post processing, but I am having trouble reading the .log file to determine metadata parameters to calculate beat frequency, range (resolution) etc.
For example, in the following few lines from one such log file, the FrameConfig line matches up quite nicely with the corresponding section in the radar studio gui for the start and end tx, 32 frames and 8 chirps, but the periodicity argument doesn't make sense to me. Furthermore the profileconfig line presumably has information regarding the start frequency, slope, idle time etc. but several of these arguments are not immediately apparent to me. I believe I programmed in a start frequency of 77 GHz and a Slope of 29.982 for example.
I know I could just write down these parameters on a piece of paper when I program them in, but being able to read them from the log file would be so much cleaner.
Any advice would be greatly appreciated
-Mike
14-Mar-2019 12:28:01: API:ProfileConfig,0,1435384036,10000,600,6000,0,0,621,0,256,10000,0,0,30,0,
14-Mar-2019 12:28:16: API:ChirpConfig,0,0,0,0,0,0,0,1,0,
14-Mar-2019 12:28:40: API:EnableTestSource,0,1,0,
14-Mar-2019 12:28:40: API:FrameConfig,0,0,32,8,400000,0,512,0,
14-Mar-2019 12:28:40: API:AdvancedFrameConfig,1,0,0,0,1,8,400000,0,1,1,400000,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,32,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,
14-Mar-2019 12:29:01: Selecting ADC Device : ,AWR16xx_lvds_4Channel_ddr_4bit_par_centre_16_bit,0,
14-Mar-2019 12:29:01: Setting the number of samples to 131072.,0,
14-Mar-2019 12:29:03: Setting the sampling frequency to 7500000.,0,
14-Mar-2019 12:29:03: Setting the input target frequency to30000000.,0,