This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Dear all,
I know you have seen many asked questions from me, I m trying to speed up my work on awr1642boost for a DEMO using CAN Interface. After solving many issues concerning can data over can bus lab, today I'm receiving classic CAN messages correctly but I need to understand and interpret CAN data. I'm looking for getting in addition of (X,Y) scatter plot the velocity of detected targets.
I'm wondering if someone here had generated the dbc file or had arrived to interpret CAN messages?
Thank you
Hi,
I assume that you are using the following demo:
mmwave_automotive_toolbox\labs\lab0005_object_data_over_can
This demo is based on the mmWave SDK demo v 2.1.0.4.
The only thing that was updated was
Knowing that, the documentation of the output data format provided in the SDK 2.1 applies for this demo.
This documentation can be found in:
Section:
"Output Information Sent to Host"
file:///C:/ti/mmwave_sdk_02_01_00_04/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html
The buffers sent are defined in "MmwDemo_dssSendProcessOutputToMSS()" see file
mmwave_automotive_toolbox\labs\lab0005_object_data_over_can\odoc-target\dss\dss_main.c
So, when you receive the CAN data, you need to first identify the magicWord header. This will be the beginning of the frame
thank you
Cesar