Other Parts Discussed in Thread: AWR1642, TIDEP-0092
Hi,
The AWR1642 requires 4 rails 3.3 V, 1.2 V, 1.8 V and 1.3 V. The TIDEP-0092 has a 5th rail called VPP-1P7 forwhich is the voltage supply for fuse chain that is supplied from the 5V_IN via ultra-low noise LDO called TPS79601DRBR (U11). What's the current requirement for VPP_1P7? What's the max noise thresholds for VPP_1P7? Can this be supplied by any of the 4 rails going to the AWR1642?
The same TPS79601DRBR LDO is used to source 3.3V to TM4C1294NCPDTT via 3V3_BRD pin. Can this supply be sourced from the other available 3.3 V within the board? What's the current and ripple voltage requirement for this supply?
Thanks,
John