1. In TMP468 application , How can i select a temperature sensor? datasheet says MMBT3904LP . this is a common NPN transistor ?
2. if just use this type of NPN , how does it install in a application ? for example, a heatsink surface, a speaker magnet surface, a chipset surface , a power mosfet surface, just glue the transistor on the heat source?
3. if the connection cable is 3~3 m length , it need any compensation components before PIN D+ /D-?
4. How to select the tie point for all 8 channel D- , the D- connection point is located closed to pin D- , or any else location ?
Thanks!
Meican.