Other Parts Discussed in Thread: OPT3004
According to the datasheet OPT3001 should match human eye frequency response. I designed a board using OPT3001 with IR LED from OSRAM (SFH 4770). OPT3001 is used for sensing if there is enough visible light to switch on/off IR LED for security camera. However when IR LED is turned on the OPT3001 immediately return numbers about 3500 lux whereas with LED off it is reporting 300 lux. From what I see frequency response is nowhere near the advertised in datasheet (LED is 850nm). Is there anything I need to configure in the driver to change the frequency response to reject IR light?
Thank you in advance.
Stepan