Is there any DRV5xxx hall sensor working at 180 degree ambient operating temp? the application is for the servo motor.
It seems the E version can work up to 150degree only.
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any DRV5xxx hall sensor working at 180 degree ambient operating temp? the application is for the servo motor.
It seems the E version can work up to 150degree only.
Regards
Brian
Brian,
Unfortunately we do not currently make any devices that are rated for >150C operation. Is there any way inside of the application to combat the ambient temperature?
The device is inside linear motor, the motor operated in 165C [peak may be up to 185C, thanks.
Regards
Brian
Brian,
Understood. Unfortunately if they have to have a solution that falls in this rating, we don't have any solutions that I can recommend. Note that the 'E' version of the device has an absolute maximum temperature of 175 deg, but this is simply a buffer to protect the device, and we do not guarantee linear operation beyond the specified operating range of 150C.