This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the impact of setting a frame trigger delay when using HW_TRIGGER mode?
I would like to use HW_TRIGGER mode with a frame delay. My understanding is that these are equivalent modes:
1) Sending the HW_TRIGGER pulse at time 0, and applying frame trigger delay = 5us
2) Delaying the HW_TRIGGER pulse by 5us in the host, and applying frame trigger delay = 0us
Thank you for your help.
Antonio
Hi Antonio,
The AWR1243 will be ready to accept a new trigger one programmed "Frame Period" after the previous externally provided hardware trigger pulse.
So if you wish to provide the HW_Trigger pulse 5us delayed in the host, with a 0 frame trigger delay, please ensure that the programmed frame periodicity is reduced accordingly to make sure the AWR1243 is ready to accept the new trigger.
Best Regards,
Anand
Hi Anand,
Thanks for your response. To clarify - in the attached diagram:
my understanding is that it is ok to have different time between external frame trigger, as long as the device frame-periodicity is programmed to the minimum. In this example, frame-periodicity <= 10.5ms. Is this understanding correct?
Thank you,
Antonio
Hi Antonio,
This understanding is correct.
Note however that the device is no longer in low-power mode once it is waiting for the external hardware trigger, and delaying the hardware trigger indefinitely may not be a good idea. We do not extensively test for conditions where the hardware trigger is provided far from the expected frame periodicity.
Best Regards,
Anand