When installing the fixing bracket of IWR1443 and DCA1000 EVM, I accidentally let the components on IWR1443 board fall off (possibly the chip resistance), The exact parts impacted is shown in the green box in the photo.
Now I am doing the experiment of collecting ADC data with IWR1443 and DCA1000.Would it affect the experiment without the two components?
If I continue to use it, will it cause the radar board to burn? If not, how can I apply for after-sales maintenance?
(Because the components fall off, I dare not turn on the power for fear of more serious damage to the board.)