Other Parts Discussed in Thread: TMP121,
Hello,
Can TMP121's IBIS model be used for TMP123? It seems the chips are similar and the only differences are pinjs 1&2 (which are gnd and NC) as well as temp range
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Elisha -
The experts on this device are out on holiday at the moment, but after looking at the datasheet I think this is a reasonable assumption you have made and it should be OK to do this, as the devices share a datasheet and as you pointed out, have only slight pin-out and performance differences, etc.
Hi Elisha,
Yes, you can use the TMP121 IBIS model for TMP123.
thanks,
ren