Other Parts Discussed in Thread: LDC1101
Hello,
I'm having issues connecting the LDC1101EVM to PC.
The drivers are installed correctly because I'm able to see that the COM port is recognised as "EVM"
I have also installed the fix patch suggested in other similar threads. The GUI is able to see the device but it is not able to connect and the "Texas Instruments" logo in the bottom right corner goes on blinking in green to the bitter end.
I am experiencing the same issue with both Windows 10 and Windows 7.
Is there anything else I could try?