I am currently using an NTC thermistor, what changes do I need to make in order to use a TMP61, TMP63, or TMP64?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMP61, TMP63, and TMP64 are footprint compatible with 0402 and 0603 packages, use the same biasing circuit and therefore will not require a board layout change. If using a lookup table (LUT), you would need to input the new Resistance-Temperature(R-T) table values that can be found in our Thermistor Design Tool. If using a curve-fit equation, the tool provides all the coefficients and example code to minimize your design time.